This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24770: maximum duty cycle

Part Number: BQ24770

Hi team,

What is the maximum duty cycle of bq24770 for 4-cell battery (4.2V/cell) application?
How much minimum input voltage is required for proper operation? Thanks!

Best regards,
Sam Ting

  • Hey Sam,

    For the converter to operate properly, the VCC voltage must be higher than the VBAT voltage by the EC table parameter V(VCC-BAT_RISE). 

    You can also refer to section 8.3.2 Adapter Detect and ACOK Output in the datasheet as the ACOK requirements match the input voltage requirements related to VCC.

    Regards,

    Joel H