For flashing the golden image generated using the code, we are referring to the document no - slua801.pdf. I am attaching the document for the reference.
In this there is sample code given for linux at the last. From this I came to know that we need to implement the flash stream parser function which is the gauge_execute_fs () function given in the document. Now in the sample code given, there are two functions gauge_read_data_class(pHandle, DC_STATE, pData, DC_STATE_LENGTH); and gauge_write_data_class(pHandle, DC_STATE, pData, DC_STATE_LENGTH) after the gauge_execute_fs ().
My question is do we need to implement those two functions as well for flashing the golden image data. I have implemented parser function which is the same gauge_execute_fs() function. Please guide me on this.
I am also attaching the reference document.6644.slua801.pdf
Regards,
Mahek