This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD25501F3: CSD25501F3

Part Number: CSD25501F3
Other Parts Discussed in Thread: CSD17581Q5A

Hi Team,

I want to use this PMOS as attached:

CSD25501F3.docx

  1. What’s the max current that can flow in the Diode and for which power dissipation it can handle? it’s not mentioned in the data sheet (need support 1.5A for 30 seconds)
  2. Do you have Spice model of this part?

Thanks,

Shlomi

  • Hi Shlomi,

    Thanks for promoting TI FETs at your customers. In theory, the body diode can conduct the same maximum current as the FET channel. However, there is a constant forward voltage drop for the diode that limits the maximum power that can be dissipated by the device. The maximum continuous current and power dissipation specified in the datasheet are calculated values as detailed in the blog below. We can use the same approach for the body diode. For the minimum pad, the typical thermal impedance is 230C/W and the maximum power dissipation can be calculated as follows: PDmax = (TJmax - Tamb)/RthetaJA = (150C - 25C)/230C/W = 0.54W. This needs to be adjusted for higher ambient temperature and for different pad geometry and board stackup that can change (raise or lower) RthetaJA. In practical designs, 0.5W max power dissipation is a good guideline. Please see the technical article below. The body diode forward voltage drop at 1.5A and Tcase = 125C is about 0.7V which gives a power dissipation = 1.5A x 0.7V = 1.05W. I think it is going to be difficult to dissipate this much power in the package for 30s (which can be considered DC or continuous).

    Welcome back, fellow FET enthusiasts to part three of the " Understanding MOSFET Data Sheets " blog series! Today I’ll be talking about MOSFET current ratings and how they’re not real. Ok, so maybe a better…
    By in Technical articles > Power management

    Other Parts Discussed in Post: CSD17581Q5A When starting a new design, engineers are often overwhelmed by the number of package options for power metal-oxide semiconductor field-effect transistors ( MOSFET…

  • Hi Shlomi,

    I forgot to attach the unencrypted PSpice model. It is in the attached zip file.

    CSD25501F3.zip