Hi,
I am facing few issues in dealing with the, High temperature GPC test. As per the manual I need to perform low current and and high current discharge at 45 deg C on my Battery pack. But the Over temperature 60degC protection set in the GG ASIC is triggered before I can complete my data logging. So this affects my data matrix in the high current and high temperature region. I would like to know if there are any other ways to solve this. I see below two options for solving this:
1) performing the high temperature discharge test at lower temperature than the proposed value: 35 deg C so I don't trigger OTD cutoff.
2) I can reduce the high current setting to much lower value so that it takes longer for the Battery cells to heat up and I could finish the test.
Can you please inform me on the effects of above mentioned solutions in regards to the accuracy of SOC calculation by my BMS.
Thanks!