Hello,
We have designed a standalone 2 layer charger board based on the BQ24650 EVM layout. All the layout is as per the recommendations in the datasheet / EVM.
Panel Input: 19-21V
Battery: Li-Ion 14.8V / 12AH
All the Test Point / voltages are as per the test procedures. The battery charging current is set a 1A for now. The board is working fine and the charging is operational for the set values. The Charging Mosfets are working fine and there is no heating observed. However, the Charger IC BQ24650 is getting heated up to 60'C. The thermal pad is very well connected to ground plane and there is sufficient ground plane on the PCB.
If the Charging current is increased to 2A, the device is getting quite hot, but the MOSFET temperature is quite normal. Please confirm if this behavior is normal or there is some issue that we need to look into.
Thanks,
Rajesh