Part Number: TPS55330
Other Parts Discussed in Thread: TPS55340, TPS61178
Hi gents,
I'm using the TPS55330 on my design to generate 15V from a 3 to 4.2V input.
Is there a way to calculate the maximum output current that my design can provide? on the datasheet § 8.2.2.5 Computing the Maximum Output Current, can I use this formula? if yes I do know the value of ηEST.
If somebody can help
regards
Bruno