Dear Support,
My customer intend to use our boost with a battery connected on Vin and a 3.3V applied on Vout.
At that time, the boost is put in shutdown with an external signal.
In such a case, when an external voltage is applied on the output, it will duplicate the 3.3V to the input, right?
Are there some limitations or damages that could occur on our boost?
Regards,