This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPROT (Fuse) Control for BQ78PL114

Other Parts Discussed in Thread: BQ78PL114, BQ78PL116, BQWIZARD

In the document SLUA537–December 2009 bq78PL114 System Design Guidelines.  I found that The chemical or thermal fuse option is commonly available in applications up to maximum voltage of 32 VDC and currents up to 12 A. So I want to konw whether this feature is not available when Pack Volatage exceed 32V or current exceed 12A, at the same time how about BQ78PL116 of this feature.

Thanks

Sam

 

  • The feature is still available in the '114 or '116 (for any fuse rating) but I don't think there aren't chemical fuses available for voltage/current levels that high.

  • In very high power applications, the FUSE (SPROT) condition can be considered a Permanent Failure condition since controllable fuses are not really used.  Once this condition is reached, the bq78PL116 is latched just like a fuse.  THe only way to get out of the condition is to remove the fault and send a Reset Fuse Command with the bqWizard or API.