Dear Experts,
Currently working with GPS Tracking for Vehicle i am using lmz34202 for power supply, i want to replace the module with the best regulator
Note: that regulator support 4v to 20v input is enough
current rating is greater than 3A,
the output voltage is 4.2V
the regulator must give a constant output voltage that doesn't swing or varied output depends on input voltage