Hi,
I using LM5365-Q1 regulator in my design. The design parameters as follows:
1. Iin (Current input) --- 470mA
2. Vin (Voltage input) ---- 24V
3. Iout(Current out) ---- 1.8mA
4. Vout (Voltage out) ---- 5V
5. Efficiency ---- 80%
6. Power Dissipation --- 2.25W.
I am doing thermal simulation for my board below are my Boundary conditions:
Ambient Temperature --> 25 degree C and Air velocity --> 0.1m/sec (19.685 ft/min). The system is In rack placement. My board is placed between two boards. The power dissipation of the adjacent boards are 3W. I am observing Junction Temp. ---> 127 degreeC.
1.The Junction Temp. is exceeding more than expected value. Did I wrongly consider any parameters ?
2. I have considered Theta jc top (junction to case top) ----> 14.2 C/W. Should I consider Theta jc (top) or Theta jc (bottom) for my simulation ?