This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24630: Charge state flashing with batteries under about 55 degrees F

Part Number: BQ24630

One of our customers has asked us to solve a problem.  It seems that of a batch of chargers and batteries we were supplied, most batteries cause the charger CHARGE state to flash at about a 1 second rate.  When looking at the charge status pin, the on time varies with battery and temperature and is always shorter with a colder battery  As the battery warms up, the ON time gets longer then eventually stays on above a certain temperature.  This GOOD temperature varies with the different battery and charger combinations.

When looking around with a scope probe while the chargers are flashing, it would immediately stop flashing when I got to the VFB point.  When removing it, it goes back to flashing.  Normally, I would minimize any capacitance around any feedback path like this, but I see that the evaluation board seems to have purposefully added capacitance at that feedback point.  There are relative large copper areas at the junction of the feedback resistors.  That would add capacitance at that point.  My estimate would be about 4-5pF.  If the reference design of the evaluation board was optimized with 22pF in parallel with the top resistor, then I should probably add 5pF across the bottom resistor to compensate for the lack of capacitance due to the lack of "extra" copper at that point on the design I have.

Another possibility would be to reduce or eliminate the 22pF across the top resistor since the design I am working with has minimal extra copper at that point.

Any thoughts?  I will try adding 5 pF in the equivalent position of C31 in the evaluation board and re-run my tests  My previous tests were done between about 45 degrees F and about 55 degrees when they all worked OK

  • Hi Skip,

       To debug this STAT flashing, can you show me waveform of VCC, SRN, STAT1 and TS voltage? Just to confirm, only STAT1 is flashing while STAT2 remains off correct? This would mean the charger is entering and exiting a fault condition (Refer to Table 2 of datasheet for possible fault conditions). I wouldn't worry too much about the capacitance of the VFB node just yet. It is a sensitive high impedance node, so putting a scope probe in parallel with it could change what the charger is actually sensing at VFB. This is why I have you probing SRN which will essentially tell me the same information.

    Thermistor in the resistor network at TS converts the temperature into voltage which is what is sensed at TS. When referring to temperatures, can you refer to them in the voltage measured at TS?