I am using the LM5118 in buck / boost configuration with an input voltage range of 8.5-32V & an output of 12V @ a 4A max load. During my testing I have forced the LM5118 into an over current fault and the regulator shuts down as expected. I am having issues with the LM5118 starting back up once the fault is removed. If my input voltage is lower than the 12V output (boost mode) the regulator recovers fine. If my input voltage is higher than the 12V output (buck mode) the regulator will not recover. If I lower the input voltage while in a buck fault the regulator restarts fine. Cycling power on the regulator allows it to recover and run fine. During the fault, Vcc is at 6.9V, the UVLO is 0.25V.