This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131: 1A positive & negtive rails.

Part Number: TPS65131


Hi Team,

One of my customer required device to generate +/- 5V/1A rails. They are referring to ADP5071 and requests similar device, do we have any equivalent device or road-map for same.

Regards, Shinu Mathew. 

  • Hi Shinu,

    Thanks for your question. Let me contact the expert for this part. You can expect a response by 1/28/20.

    Best,

    Grant

  • Hi Shinu,

    How much current TPS65131 can deliver to the load is a function of, among other things,  input and output voltage. you mentioned that output voltage is +/-5V and assuming 3.3V input voltage, maximum load current from VNEG supply will be ~600mA. This is limited by the internal switch current limit. Unfortunately, we do not have a device in our portfolio with similar specifications as competitor device you mentioned.

    Kind Regards,

    Liaqat