Hi,
My project is:
Vin =24Vdc stabilized, Vout=12 Vdc Iout from 500mA (st.by) to 10Amp full load
I attach the schema of the board i'm debugging.
I checked the switching waveform at the input of LC filter (out of half bridge) and I found that in no load or light load
i get a pattern of 24Vdc for 2us and 0Vdc for 1.6us and in this situation the Vout is corect 12Vdc
When I apply the full load (this means tha a square waveform 220kHz is applied at the H brigde in the upper side of the schematic
the Vout drop at 9Volt and the pattern of voltage at the out is 24Vdc for 2.24 us after 0Vdc for 1.32us after 24Vdc for 400ns and 0Vdc for 3,24us
this pattern repets itself till the load is in after come back to the previous.