This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200: HOW TO USE TPS61200? SHOULD I GIVE ANY EXTERNAL CONNECTION TOO APART FROM INPUT AND OUTPUT?

Part Number: TPS61200


I want a boost ic which can boost 0.3V input which comes from vibration energy and current with hardly 10mA. Will this product be helpful for me? How should I handle this? Is it enough if I give input voltage to input pin and get output voltage from output pin?