This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best method for 0-100% regulating heat load on 230VAC with low harmonics requirements

Hello

in our application we need to precisely control a 230VAC resistive heater coil load (air cooled with a large air flow) from a 230VAC/50Hz 1 phase circuit with a max power of 3.3kW (16A). The 230VAC input side must be power factor corrected and should have less than 5% THDi. There is no isolation requirement for the load.

The resistive heater coil load has to be regulated from 0-100% in about 1% increments (7 bits 0-127 are fine). The regulation normally ramps over a couple of seconds but can also jump at 50Hz The output of the controling MCU is a proportional PWM 0-100% signal (it could also control a resistor network or write the value through I2C/SPI).

Simple circuits lilke triacs can't be used as phase cutting produces to many harmonics. Also half wave switching can't be used as the AC load must be continuous with each cycle. The load is to be used behind inverters (e.g. solar and ups).

Research has shown a number of approaches:
 diode full bridge rectifier with PFC and variable DC/DC converter
 fully controlled igbt full bridge with AC chopping (5+ kHz) and duty cycle control
 fully controlled igbt half / diode half bridge with AC chopping agin
 and possibly others

The possible tropologies are quite a few. What I'm looking for is a suitable cost, parts and space efficient topology with a (single) control IC that drives the IGBTs as well as manages their duty cycle and PFC based on the MCUs proportional load output. The efficiency is secondary as the switching losses can be damped into the airflow together with the heat load.

Most designs and evaluation modules are intended for a fixed voltage (CV) output instead of a variable voltage with constant current (CC with a constant resistive load). The ideal IC / topology could operate in constant power mode, however that would be only icing on the cake for a small premium.

Any pointers and discussions for suitable topologies, TI power controller ICs and reference designs is greatly appreciated.

  • Hello,

    You can use C2000 series controller if you'd like to use a digital solution.

    And in this application, I'd like to recommend CCM PFC and Buck converter.  And regulate the output voltage reference to realize the constant output power control.

    Btw, do you consider a analog solution?

    regards,

    Teng

  • Hello,

    thank you for the topology suggestion which I will investigate further.

    So far we didn't consider any analog solution as the application must not have any mechanical input or actuators. I'm not aware of other analog solutions for 230VAC. Using a linear mosfet as in DC load application doesn't seem appropriate and also rather expensive. Do you have another analog solution in mind?

    My background is PLC which is 24VDC and typically 4-20mA / 0-10V / PWM and binary input output. AC power electronics is still a bit unfamiliar while learning.

    Thanks,

    André

  • Hi  André,

    I am not sure if PLC can do this work. Anyway C2000 is recommended.

    In the analog solution, it still needs to change the divider resister value to regulate the output reference.

    Regards,

    Teng