This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck design using mosfet switch

Hello all

In one of my application i need to design the buck regulator circuit with the following specification

1.Input voltage 12V

2.Output voltage 5V

3.ouput ripple voltage 50mV

4.Load current 200mA

5 switching frequency 2Mhz.

Any other parameters from the microcontroller to driver circuit could be assumed.

I need to design the buck converter using mosfet switch,please any one guide me on the design of mosfet driver circuit,also gate resistor calculation for the mosfet.