This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53681: Behavior in Light or No-Load condition

Part Number: TPS53681

Hi,

What is the behavior of this IC in Light or No-Load conditions. Weather the efficiency and other thing will be changed??

  • There are NVM settings in this device to operate (1) all phases, forced CCM mode, (2) dynamic phase shedding, CCM mode, phases will drop based on configured thresholds when the output current is low, and (3) auto-DCM mode, similar to dynamic phase shedding, but also enable diode emulation in 1 phase mode. 

    You can refer to the description on pg 88 of the datasheet and the TRM document describes the register settings. 

  • Hi Matt,

    What is auto DCM mode and how to activate that mode?

  • Auto-DCM is a diode emulation mode. This means at light load below the critical conduction point, (e.g. when the inductor current would be going negative in FCCM mode), the controller will sense when the current is reaching zero and turn OFF the low-side FET, using the body diode of the FET as a diode rectifier. This increases light-load efficiency because turning off the low-side FET will prevent the power stages from sinking current, and keep the output voltage at the regulation point higher - So the converter will need to send pulses less often to keep the output voltage in regulation - hence reducing the switching loss. There is an OK description in this document from TI: https://www.ti.com/seclit/ug/slyu036/slyu036.pdf around pgs 16-18 showing power component waveforms. 

    To try it with TPS53681:

    • MFR_SPECIFIC_15[PAGE = 0x00 or 0x01][15] bit to 1b to enable DCM mode in 1 phase operation
    • MFR_SPECIFIC_06[PAGE = 0x00 or 0x01][15] bit to 1b to enable DCM through tri-state PWM operation.
    • MFR_SPECIFIC_14[PAGE = 0x00 or 0x01][7] bit to 1b to enable dynamic phase shedding. 

    These should all be accessible through the Fusion Digital Power Designer GUI. 

  • Hi Matt,

    I need one more clarification regarding programming the NVM in TPS53681.

    Is this device comes with the Secured NVM or Once after programming only it will be secured?

    If it comes with secured NVM, How to reprogram the device from default values? 

  • TPS53681 ships with a set of NVM default values as described on pgs 46-48 of the datasheet. 

    The NVM is re-programmable > 1000 times as it is an EEPROM Technology. 

    pg 94 of the datasheet describes the process to lock NVM programming with a password, with the NVM Security feature.