This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: Switching Waveform

Part Number: TPS61022

Hi 

I use TPS61022 as booster from 3.7V Lipo battery to 5V and it is in PWM mode

The steady state current is around 360mA. RMS with around 1.2A maximum current at start.

I measured the Vout in AC coupling and I have ~40mV spikes@1MHz.

Can I improve this noise?

Can PFM mode improve it?

What is a the current range which is considered light mode?