Other Parts Discussed in Thread: GPCCEDV, BQ25703A, BQSTUDIO
Hi
I have run the GPC cycle and am trying to update the FCC. I charge the device up until VCT is high. I then discharge the batteries until max. I am using 18650 cells that have an internal protection circuit that cuts out at 2.8V. I am discharging the batteries down until they cut out. This is causing the device to reset. Am I right in thinking for the MaxError to update, I need to stop the discharge before the protection circuit cuts out?
Also, I ran the GPC cycle discharging from about 4.15V per cell. For the device, we want to extend the battery life, so want to charge to 4.1V and discharge to 3.3V. I want the SoC to go from 0% to 100% between those cell voltages.
Can I run a discharge to update the FCC, then enter that value into the Design capacity? I will also update the charging voltage values for all temperatures in advanced gauging algorithm. Are there any other registers I need to set to adjust SoC limits?
Thanks