Other Parts Discussed in Thread: BQ25895
Hello,
I need some help with my component selection for a Li Ion battery charge IC with a dedicated power path for the system. We at Greenlee are not battery experts and this would be our first time designing for a Li Ion battery. Find below our application requirements:
1. Battery: Single cell Li Ion 1S1P; 3.6V, 2.9 Ah (Max fast charge current: 1.5A)
2. System load 150~250 mA
3. Input power: Single USB type C connector.
Host device is required to identify the current input source and modify current limit accordingly. Additionally, battery temperature and battery charge status need be identified by the host device.
Based on these limited specification, what is my best option between BQ25619 and BQ25895.
Any help is much appreciated.
-Satish