Part Number: BQ2057W
Other Parts Discussed in Thread: BQ24005
Good afternoon,
I am looking to use BQ2057W to charge 8.4 volt Li-ion battery .There are a no.of issues that I faced:
a)I Used 0.2 ohms as Rsns in high side voltage sensing configuration. The current drawn was only 200mA and the voltage across Rsns was only 40 milli volts .
b)Then I tried changing Rsns to 0.1 ohms which means the current should double to 400mA .But instead it drew only 200mA and voltage across the Rsns was 20 milli volts.
I read the datasheet and it says that it tries to maintain a voltage of 125 milli volts (TYPICALLY) in constant current mode .But I wasn't able to figure it out why it couldn't achieve that.
Second of all if Rsns is changed ,CURRENT should change and not the VOLTAGE across Rsns .But it occurred the other way round i.e the voltage changed keeping the current constant to 200mA.
I hope Experts help me out and find a solution as soon as possible.