Other Parts Discussed in Thread: MSP430G2553
Tool/software: Code Composer Studio
TPS65835 can update programs with BSL?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
TPS65835 can update programs with BSL?
According to the MSP430™ Flash Devices Bootloader (BSL) User's Guide, BSL pins named nRST and TEST.
On the TPS65835, pin 17 is nRST (Reset) and pin 20 is TEST. They both say "Spy-Bi-Wire test input during programming and test" so it seems logical to me that this integrated MSP430 device would support BSL programming.
The MSPBSL can program the MSP430G2553 so there should be no issue with the TPS65835. Per the earlier threads, I think there is a disconnect in the tool chain. Specifically, the associated linker command and header files for the TPS65835 are no longer a part of the CCS device packages. This in combination with an old FET and CCS might be the reason why the device appears to have a fuse blown. The fuse may be blown, but it is more likely that your tool chain is not compatible with device.
I would recommend obtaining the latest FET, using the latest CCS, and finally updating all of your code and projects to use the generic MSP430G2553 support files.
Regards,
Chris