This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62130A: draw more current and output not stable

Part Number: TPS62130A


We use TPS62130A to convert the voltage from 2.8V to 5V, the circuit are exactly same as TPS62130A_EVM, but it draw more current 10.8mA with 10mF load and output voltage keep jumping from 4.6V to 4.9V, any one have idea what is going on?

Thanks,

Feng