This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pusled adjustable Led Constant Current

Other Parts Discussed in Thread: LM3463, LP8556, LM3643, TPS61199

hello,

i want to search a solution (IC) from 8-16 Leds (VF about 3V /LED) in Serie on about 60V System Voltage (sinking mode)  in a range from 0.....50mA constant current (max. 100mA) and pulsed with up to 10khz..

I found the IC LM3463. The EVM Board has 200mA. Does it works with lower IC current from min. 1mA the IC LM3463? it is possible to reach a accuracy with 1% of constant current?

Would the IC be suitable or which IC would you recommend me?

Best regards

Steve