Hello team,
I'd like to improve a noise tolerance on the VR_ON input.
Could you tell if there is a hysteresis on the input and there is any acceptable slew rate range?
Thanks in advance,
S.Sawamoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
I'd like to improve a noise tolerance on the VR_ON input.
Could you tell if there is a hysteresis on the input and there is any acceptable slew rate range?
Thanks in advance,
S.Sawamoto
Hi Shinya,
VR_ON is just logic high and low. The logic low max voltage is 0.3V and the logic high min voltage is 0.8V. Usually we recommend to add a 1000pF/0402 decoupling cap on that pin. No slew rate requirement.
Thanks,
Nancy