Other Parts Discussed in Thread: BQ24074
Hi Guys
With the control pin enabled, I can verify that the 4 pulses is close to 93mA, 5 pulses is close to 187mA etc.
My issue is with the single pulse. I am trying to stop the charging, but still keep the power path management operational. What is the purpose of the single pulse? “Force Termination” Is this not to stop the charging? I need a means of switching the battery charging off, but still supplying the unit power through the charger chip.
Any suggestions appreciated.
Thanks
Rodney