Can BQ76940 be used for Lithium-Titanate Cells ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Carlos,
This device is not the best choice for these cells. The cell measurement range is specified down to 2.0V, which is close to the limit of a Lithium-Titanate discharge. In addition, the OV protection threshold is programmable from 3.1V to 4.7V, which is too high for these cells. You might instead consider the BQ76952, which is sampling now and will be in production later this year.
Thanks,
Terry