Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50
Tool/software: Code Composer Studio
BQ40Z60.
In my application, cell is charged to 3.8V(that is full charged I configure), then charge FET is open, TCA sets 1. After that, I don't discharge cell, gauging status is 5A. But Ag time to empty changes to 49020 or 39216 and doesn't keep 65535. Could you give me some advice about this phenomenon?
1, Does 'avg time to empty' only depend on 'avg current'? When avg current becomes 0, avg time to empty is 65535?
2, When cell is charged to full, gauging status sets 5A. Do HIDRV and LODRV pins change to be low and keep? In other words, high and low FETs for charger become open?
3, When does avg time to empty change to other lower number like 49020 or 39216?
4, If avg current is positive like 100mA or 2A, is avg time to empty 65535?
5, How often does avg current update?
Thanks