Other Parts Discussed in Thread: BQ40Z50-R1, BQ40Z50,
The 3 cell battery we use has an internal gas gauge based on TI bq40z50-R1. When battery is in undervoltage condition, bq40z50 disables discharge and the voltage at the battery terminal is zero. We found that we can revive the battery by taking the battery out of the system and directly applying 12V to it.
The question is how to revive the battery without taking it out of the system. Our charging circuit is based on TI bq25703A. Is there a way to force precharge mode when the battery voltage is zero?
There is a SMBUS at the battery connector. Is there a way to communicate with the bq40z50 to enable discharge so that the voltage at battery terminal is not zero? From the bq25703A data sheet, it seems that bq25703A can automatically enter precharge mode when the battery voltage is below a threshold.
Thanks,
Zhaohong