Hello,
I am currently working on a design with the TPS23755 based closely on the TPS23755EVM-894 reference design from TI.
The flyback transformer used in the EVM is the LDT0950-50 (150uH, 1 : 0.44 : 0.39).
Are there any suitable alternatives to this for a 13W 12V solution?
I am considering the Coilcraft POE13P-12L_ (127uH, 1 : 0.5 : 0.5) or the Wurth 7491199112 (127uH, 1 : 0.5 : 0.5).
These are of course slightly different winding ratios to the recommended transformer. Are they suitable?
I would also like to ask if it is also reasonable to use a smaller transformer for a 7W solution?
For example, the Coilcraft POE70P-12L_ (155uH, 1 : 0.667 : 0.667).
Thanks in advance