Dear Sir or Madam,
we built the reference circuit for the LM7461 for polarity protection. We double checked the correct wiring multple times, our build is a double sided PCB with SMD components.
The output is 12V or -12V depending on the applied polarity. We can remove the MOSFET and the LM7461 still conducts both ways. There is no polarity protection that can be observed.
Our input is 12.6V and the intented purpose is to protect a buck converter that is connected to a microcontroller.
Attached is our Eagle schematic and board. At this stage, we have stuck experiencing the above situation.
Thank you,
Daniel