Other Parts Discussed in Thread: LM5170, LM5170-Q1, LM5176-Q1
Hi,
I recently bought LM5170EVM-BIDIR to check that if i can use it implement a battery to battery charger. Required charging currents are 30A and 45A. Is it possible to use this devkit as a buck-boost. Where I can get 14.5V as the output if the input voltage varies between 8V and 16V?
Additionally how can I control the output current?