This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5036: EN pin controls just the digital interface block or does it control the entire LP5036 chip

Part Number: LP5036


Hi,

On page no 12, in the functional block diagram, the EN signal is shown as an input to the digital interface. And on page no 19, it is mentioned that in SHUTDOWN state, when EN=L, the Icc is less that 1uA. Does this mean that in SHUTDOWN state when the EN=L, all the blocks of LP5036 like Bandgap, LDO, Oscillator, IREF setting current etc are disabled? 

Also, if say Vcc is connected to 3.3V and EN=L. Now if EN is made high, could you please let me know what is the time taken by LP5036 to shift from SHUTDOWN state to initialization state?

Best Regards,

Bhargav