Hi! I am trying to design a layout for the TPSM84424. I used the EVM to evaluate it and thought the performance was good for my application.
I noticed that some EVMs for other parts have gerbers posted online. I would like to use the TPSM84424-EVM design as a starting point, but some of the traces shown in the User Guide are a bit blurry. Is it possible to get gerbers for this module (or Eagle files if by chance that's what you used)? Alternatively, there is a sample layout given in the spec sheet for the TPSM84424; gerbers or CAD files for that would also be super helpful as an alternative, since the parts I am confused about are the same on both of these layouts.
I was also wondering if you have any advice for designing a layout for a 2-layer board. The recommended layout seems to be a 4-layer board where one layer has an AGND plane and 3 layers have PGND. WIth a 2 layer board, I only have one layer that can have an uninterrupted plane. I could try to split the bottom layer into two localized planes, or I could try to do one of the planes on top, working around the part and all the top traces, and it would just have to cut the other plane with vias and bottom traces when I need to route it. I don't know how feasible either of these solutions are; it looks very difficult. What would you recommend, or do you think this is a part that requires 4 layers?
Finally, I noticed that it is recommended to use AGND with analog circuitry since PGND is noisy. However, the EVM and spec sheet diagrams seem to imply that PGND should be the return path for VOUT. My circuit is basically analog (with a few ADCs thrown in) so should I use AGND or PGND with the rest of my circuit?
Thanks!