This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24080: Charge Done State never show up (Status LED, STAT2 pin)

Part Number: BQ24080
Other Parts Discussed in Thread: BQ24314, TPS61022

Hi,

I'm using a bq24080 connected directly after a BQ24314 and the charge done state nerver come up even if the battery is full charge. However the charge conditions are met : I(term) is lower then 100ma, in fact it is way lower it is more like 0.07mA. (specsheet equation #4 page 11).

Is there something i missing?

Thanks for any help.