This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28064A: Recommend PFC for three phase and high Vout solution

Guru 19645 points
Part Number: UCC28064A
Other Parts Discussed in Thread: UCC28180, , UCC28070A

Please let me know about recommended PFC: UCC28180(CCM) or UCC28064A(TM) for below condition;

①About 3-phase input: 200Vac solution, Which is recommended PFC, UCC28180 or UCC28064A?

 Or, isn't 3-phase relation for PFC choice and depend on only output power?

②About High Vout: 750V solution (input is single 85~264Vac), is UCC28064A have any problem?

Best regards,

Satoshi