Other Parts Discussed in Thread: TIDA-00443
Hi Experts,
I show UCC28180's datasheet 8.3.14.
I understand purpose of this diode and spec of Vf should be between -0.438V and -1.1V at all temperuture condition.
Could you please give more explanation what kind of Vr and If is required?
For example, is
MMSD4448(ON semiconductor) recommended?
www.onsemi.jp/.../MMSD4448-D.pdf
The Vf of the diode is between -0.6V(at If=5mA) and -1.0V(at If=100mA).
This is Small Signal Diode, Vr=100V and If=200mA.
Regards,
Terazono