Tool/software: WEBENCH® Design Tools
Hello
I'm trying to design a power supply based on the LM5022 chip.This design has an input at 48V and an output at 120V 2A. In the Webench tool, no MOSFET is suggested, nor is it possible to add one manually (I couldn't find how).If i lower the output current to 1A a MOSFET is suggested but it is still not possible to add others that are not listed. Can you sugest a way to get around the problem ? or another tool that allows me to select an appropriate mosfet and adjust the LM5022 circuit to work with that MOSFET.
thanks
Pedro Peixoto