Other Parts Discussed in Thread: ALLIGATOR
I have two designs which are almost exactly the same, but one of them is over currenting. The older design works, but the newer one over currents. I see the high side MOSFET is heating up, but I don't see the inductor for regulating getting hot and also the low side MOSFET isn't getting hot. I'm using a V62/13607-01XE on the original design and TPS40170MRGYTEP on the new design. Are these chips the same?
I also notice on page 30 of the datasheet it talks about LDRV Gate Capacitor, but it doesn't give any information about how to pick the size of the cap. It also says the cap should be between the LDRV and GND and then refer to reference [1] later in the datasheet. Would this cap just be connected to the LDRV pin and GND and how would I determine the size of the cap? I also believe Cgs < Cgd is true for the MOSFET. Could this be causing the over current due to some shoot through and/or maybe the MOSFET isn't turned all the way off?
Or on page 16 of the datasheet could the overcurrent protection not be right for the chip? The datasheet I'm using is at this location http://www.ti.com/lit/ds/symlink/tps40170-ep.pdf. Also, the output of the chip is a little higher than what it's suppose to be by 0.2 VDC.