When in shipping mode (REG07[5]=1), with a charged battery attached but VBUS disconnected (physically), which battery quiscent current should we consider?
In the datasheet I note there is the case with max 5 uA, specificed for V_VBUS < V_UVLO. Then there is the case with max 20 uA, specified with 'no VBUS'. The latter sounds more like VBUS disconnected to me, but I must have misunderstood something, because it does not make sense to me that the battery quiscent current would be higher when VBUS is disconnected than when it is connected with a low voltage (<V_UVLO).
Thanks!