Hi FET team,
Asking a question from a customer-
I have to super caps in parallel. One is a 3F and the other 0.5F. I charge the small cap first to 1V. The big cap has this FET in series as a switch to GND. When the first small cap reaches 1V, I turn on the FET essentially connecting them in parallel. There will be a large current initially an then decays when equilibrium is reached at 167mV roughly (1/6)V.
The total series resistances are 0.3 ohm for the 0.5F cap and 0.07 ohm for the 3F cap. The FET is 44mohm according to the DS.
I turning on the FET with 3.3V VGS.
This part is very attractive for its small size although the max. sustained power dissipation is only 0.5W.
I can afford to add an additional series resistance but probably no more than 1-2 ohms.
The other thing I could do which I much rather do instead of adding series R, is to slowly turn on the FET by putting a large RC time constant on the gate thus increasing its RDSon and limiting the initial current spike.
What would you recommend?
Thanks,
Lauren