Hi Team,
We have a customer inquiry below about the LM117 performance at high temperatures:
Our customer would like to know if do we have data or test results of the behavior of the component at high temperatures (always within the T range -55° to +125°C). They are particularly interested in knowing if we have detected any anomaly during its performance at temperatures closer to higher limit. They are afraid that the temperature their unit can reach a certain point may be affecting the functionality of the component. In any case, they are above +125°C though.
What would be the thermal impact on the component jitter? Could it produce an extension of the duty cycle?
This is for a space application.
Please let me know if you have a question with the customer.
Thanks!
Jonathan