Part Number: BQ2022A
Hello experts,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ2022A
Hello experts,
Hi Ryo,
The SDQ line is used for both communication and programming. SDQ operates at 3.3V for a high level for communication, but goes to 12V for programming. During programming the MCU must be protected from the 12V if needed. The right 100 ohm limits current into the 5.6V zener diode. The left 100 ohm limits current from the zener clamp level to the MCU. Other circuits which allow bi-directional data while limiting the voltage to the MCU should also work.
Information on communicating with and setting the BQ2022A is described in the data sheet, see section 7.5.
Hello WM5295,
Thank you for your comment.
I understand the details.
Thanks and best regards,
Ryo Akashi