Hi,
I am trying to do a current LED driver using TPS40192. I need use PWM for dimming the output. I tested some ideas, but I didn’t get a good result.
Features
• 10-V to 14-V input range
• 13.5-A fixed output, with 200Hz PWM dimming (0-100%)
Could I use the EN pin to do this? I think that the startup sequence time (6 ms) does not accept 200Hz.
There is another way to do this?
Danilo Americano de Carvalho