Hi, I'm working with a bq24610 EVM. In the user guide it lists the battery charge current as 2 A min, 3 A typical, and 8 A max. The cells I am using have a recommended charge rate of 900 mA and a max charge rate of 1.8 A.
Can I go below the 2 A minimum charge rate? According to the bq24610 manual, ICHARGE = VISET1 / (20 x RSR). So for a 900 mA charge rate, I would set VISET1 to .18 V? Will this work?
Thanks,
Ron