This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: Can TPS63070 powered by USB +5V/500mA current?

Part Number: TPS63070

Dear TI,

I am currently using TPS63070 as my regulator for RFPA, and the regulator is powered by USB 5V/500mA.

The board also can be powered by battery from 3V to 7.4V when no USB. So I need buck and boost.

Can the TPS63070 use USB supply to regulate and maintain 5V? Or this chip is not for USB application?

BRgds

Manimaran