This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR36015-Q1: Min On-time

Part Number: LMR36015-Q1


Hi TI-team

My customer want 3.3V of Switching Frequency vs Input Voltage.

They use Vin:32V, Vout=3.3V, Freq=2.1MHz

I think under the above conditions it will be less than Min On-time.

Min On-time is 49.1ns @Vin:32V, Vout=3.3V, Freq=2.1MHz

Can you provide 3.3V switching frequency vs input voltage ?

 

Best Regards,

Koji Hayashi