This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A60-Q1: Recover time of over-current and over-temperature

Part Number: TPS7A60-Q1

Hi team,

As written in the data sheet of TPS7A60-Q1: it has over-current protection and thermal shutdown protections. 

But our customer wants to know the recovery time of over-current and overheating.

For example, the thermal shutdown  is 165℃, and the recovery threshold is 145℃.

So how long can it return to normal output when the temperature is lower than  145℃ ?  Similarly, what about the recovery time of over-current protection?

Thanks.

Best regards,

Ansel Song