Hi,
Do we have the reference number for efficiency at very light load? Currently we have test result as below, and the efficiency is very low. Is it expected result?
- Vin=14.46V Iin=0.0889mA
- Vout=3.3V, Iout=0.022mA
- Pout/Pin=5.64%
Thanks!
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Do we have the reference number for efficiency at very light load? Currently we have test result as below, and the efficiency is very low. Is it expected result?
Thanks!
Antony